Skip to main content
PJose.4
Senior
February 14, 2023
Question

Implementation of TFM_SBSFU on STM32U585

  • February 14, 2023
  • 12 replies
  • 3775 views

Hi All,

i have downloaded the STM32U585 firmware package from the official sources and want to implement the TFM SBSFU program code into my development board(U585-IOT2A) using STM32 Cube IDE. The user manual mentions installation not possible using Cube IDE and works with EWarm IAR Workbench version 8.50.9. But i am not able to download the mentioned version of EWarm IAR Workbench. Please suggest the following:

  1. Implementation support using STM Cube IDE
  2. Working IDE version of EWarm IDE.

Kindly provide assistance regarding the same.

References Used : UM2851 and STM32U585 Firmware Package

Thanks and Regards

This topic has been closed for replies.

12 replies

Semer CHERNI
ST Employee
February 16, 2023

Hello @Community member​ 

First let me thank you for posting.

If you have a newer version of IAR that the 8.50.9, you should be able to run the program with it.

The mentioned IAR version is the minimum one that support the project.

Kind regards,

Semer.

PJose.4
PJose.4Author
Senior
February 16, 2023

Hello @Semer CHERNI​ 

Thanks for your reply

Could You please suggest some solution to run the code on STM Cube IDE.

The main issue with IAR is we have to purchase a license for code size > 32kb and the SBSFU is greater than that, one of my colleague is facing errors in running the SBSFU application in IAR 9.

Please suggest implementation on Cube IDE.

Thanks and Regards

GTort.1
Associate II
February 16, 2023

hi @Community member​ and @Semer CHERNI​ 

I have a perfectly similarly question I just asked very recently regarding TFM Application from STM32U5 package

is there a way (e.g. even from the command line) to build such applications without the IAR software, which is commercial?

thanks!

Gianluca

PJose.4
PJose.4Author
Senior
February 16, 2023

Hi @GTort.1​ 

Greetings

As per my knowledge from the user manual the TFM Application wont work with any other tool than IAR and that is commercial.

I am requesting from my end to ST Official to provide a quick solution to enable the same using STM Cube IDE

Thanks

PJose.4
PJose.4Author
Senior
February 22, 2023

Hi All @Semer CHERNI​ ,

I came to know about a recent update to the TFM package that will be provided from ST Side with support for STM Cube IDE as well. Please comment if any official confirmation on this is coming from ST Side. it would be really helpful if we can get a solution so that we can implement the same.

Awaiting a reply from the community

Thanks

GTort.1
Associate II
February 22, 2023

that's what they replied also to my similar issue: by the end of February there should be a new version of STM32U5 Cube with suppport for building all projects in STM32Cube IDE

best,

Gianluca

PJose.4
PJose.4Author
Senior
February 22, 2023

HHI

We are also waiting eagerly for an update from ST side on this regard.

Thanks

PJose.4
PJose.4Author
Senior
March 2, 2023

HI All

First of all i would like to thank ST Team for providing an update on the TFM Package. I downloaded the package and am trying to build the TFM SBSFU Package with the following prerequisites

  1. python installed
  2. pip with requirements also installed(requirements.txt)
  3. python added in environment variable
  4. installed imgtool from python script

(these are taken from the readme document)

When i build the tfm-sbsfu program from stmcube ide i am getting 2 errors.

  1. can't cd to the path \..\..\..\..Middleware\Third_Party\mcuboot: no file or directory
  2. No File found - \..\..\..\imgtool\main,py: no such file

I verified the directories mentioned the 2 errors and found the files were present. due to this the postbuild.sh script is failing. (Attaching the error screenshot for reference).

I request help from the channel to know if i have missed anything.

I am refering to the readme files and UM2851- Reference Manual

Kindly assist me

Thanks in advance

0693W00000aI1xJQAS.png 

Guillaume K
ST Employee
March 2, 2023

Hello

is there a space character in the path where STM32Cube_FW_U5_V1.2.0 is installed ?

if yes, try to install it in a path where there is no space, or use DOS subst command to create a new drive letter from STM32Cube_FW_U5_V1.2.0\ and load the project from this drive (in STM32CubeIDE).

PJose.4
PJose.4Author
Senior
March 3, 2023

Hi @Guillaume K​ 

I tried building the program by copying in my c drive and a path with small text and no spaces. I copied the entire firmware folder into this path and tried building the same.

Hope this method is correct. please correct me if i am wrong.

Thanks

Guillaume K
ST Employee
March 3, 2023

did the compilation succeed ?

PJose.4
PJose.4Author
Senior
March 7, 2023

Hi @Guillaume K​ 

Following is the error message occuring pasted as plain text(in image full message wont be getting properly)

TFM_SBSFU_Build message

[arm-none-eabi-objdump -DS "TFM_SBSFU_Boot.elf" > "TFM_SBSFU_Boot.elf_asm.txt"

"../postbuild.sh"

C:/Intel/en.stm32cubeu5-v1-2-0/STM32Cube_FW_U5_V1.2.0/Projects/B-U585I-IOT02A/Applications/TFM/TFM_SBSFU_Boot/STM32CubeIDE/Release

../postbuild.sh: cd: line 17: can't cd to C:/Intel/en.stm32cubeu5-v1-2-0/STM32Cube_FW_U5_V1.2.0/Projects/B-U585I-IOT02A/Applications/TFM/TFM_SBSFU_Boot/STM32CubeIDE\..\..\..\..\..\..\..\Middlewares\Third_Party\mcuboot: No such file or directory

Windows_NT

Postbuild with python

python: can't open file 'C:\\Intel\\en.stm32cubeu5-v1-2-0\\STM32Cube_FW_U5_V1.2.0\\Projects\\B-U585I-IOT02A\\Applications\\TFM\\TFM_SBSFU_Boot\\STM32CubeIDE\\Release\\scripts\\imgtool\\main.py': [Errno 2] No such file or directory

postbuild.sh failed

make[1]: *** [makefile:96: post-build] Error 1

make: *** [makefile:62: all] Error 2

"make -j8 all" terminated with exit code 2. Build might be incomplete.]

The line 16 of postbuild.sh is throwing error.

cd $projectdir"\..\..\..\..\..\..\..\Middlewares\Third_Party\mcuboot"

the STM Cube IDE build when running cannot cd to the path in above. but the path is correct and i just verified the same with files inside the respective folder.

Is there any other thing that i have missed.

thanks for support

Guillaume K
ST Employee
March 7, 2023

This line is strange:

../postbuild.sh: cd: line 17: can't cd to C:/Intel/en.stm32cubeu5-v1-2-0/STM32Cube_FW_U5_V1.2.0/Projects/B-U585I-IOT02A/Applications/TFM/TFM_SBSFU_Boot/STM32CubeIDE\..\..\..\..\..\..\..\Middlewares\Third_Party\mcuboot: No such file or directory

in TFM_SBSFU_Boot project, postbuild.sh line 17 is :

cd $projectdir"/../../../../../../Middlewares/Third_Party/mcuboot"

So why are there backslash characters at the end of the line in your log file ? did you change line 17 in postbuild.sh ?

what version of STM32CubeIDE are you using ?

PJose.4
PJose.4Author
Senior
March 7, 2023

Hi @Guillaume K​ 

That was done for a testing purpose because windows systems uses backslash for that purpose i just changed the command in postbuild.sh script.

After changing the line 16 to

cd $projectdir"/../../../../../../../Middlewares/Third_Party/mcuboot"

the build output becomes

"../postbuild.sh"
C:/Intel/en.stm32cubeu5-v1-2-0/STM32Cube_FW_U5_V1.2.0/Projects/B-U585I-IOT02A/Applications/TFM/TFM_SBSFU_Boot/STM32CubeIDE/Release
../postbuild.sh: cd: line 16: can't cd to C:/Intel/en.stm32cubeu5-v1-2-0/STM32Cube_FW_U5_V1.2.0/Projects/B-U585I-IOT02A/Applications/TFM/TFM_SBSFU_Boot/STM32CubeIDE/../../../../../../../Middlewares/Third_Party/mcuboot: No such file or directory
Windows_NT
Postbuild with python
python: can't open file 'C:\\Intel\\en.stm32cubeu5-v1-2-0\\STM32Cube_FW_U5_V1.2.0\\Projects\\B-U585I-IOT02A\\Applications\\TFM\\TFM_SBSFU_Boot\\STM32CubeIDE\\Release\\scripts\\imgtool\\main.py': [Errno 2] No such file or directory
postbuild.sh failed
make[1]: *** [makefile:96: post-build] Error 1
make: *** [makefile:62: all] Error 2
"make -j8 all" terminated with exit code 2. Build might be incomplete.

The version of STM Cube IDE is 1.11.0

Thanks