Is there a way to use the CLI to set the security read back in the option bits and also execute the start command?
I would like to set the security fuse but also have the application start running. I can set the read protection but after that I can no longer communicate with the unit. Likewise I can start the application using the start command -s but after that if I try and program the object bytes it halts the processor.
Trying to avoid a power cycle of the board after factory programming prior to functional test.