Management of OTA download of a corrupted binary in an STM32WB BLE application
Hi,
I am currently working on a bluetooth application, on an STM32WB55 microcontroller, to which I have integrated OTA update functionality.
As Loader I used the one present in the provided code examples.
The application and downloads work properly, my question is: what happens if the binary file I transmit is corrupted?
At the moment I have run some tests. However, if I manipulate the binary file by going to delete parts or overwriting others, the trend may change. There are cases where after downloading it remains in the OTA loader and others where the firmware is loaded but the application crashes not allowing the binary to be reloaded.
So in the loader present in the examples I think that in addition to the key check there is no check on the validity of the received binary, is there?
In that sense how could one proceed? By inserting an additional check in the loader (e.g., CRC) or has some other functionality been provided?
Thank you very much