No CRC error in reception even is MISO not connected on STM32H7 SPI ??
Hello,
This question is the follow-up of this one:
I thought I had fixed it thanks to the GPIO setting but it was just bad luck.
My setup is:
- two Nucleo STM32H743
- the master is using on SPI1
- the slave is using SPI2 (with SPI1 I have no issue)
- clock setup is: for master VOS1, Sysclk 400MHz, HCLK 200, PCLK 100, spi_ker_clk 200 and SPI baudrate prescaler at 8. For master every clock divided by 2 (parameter M to setup ref1_ck of PLL1 was changed)
- GPIO: high freq / push-pull / no pull down (tried with pull down, no difference)
- slave receives correctly all the time
- master never receives answer from the slave
- SPI setup at master side to receive the answer from slave: simplex receive only, CRC enabled, datawidth 8 bits, 5 bytes to receive
I completely unplugged the MISO wire. On master side I of course still gets the EOT event (as expected) but I expect to get a CRC error since I should receive crappy data , perhaps random or all 0 bytes. But I have no error status in SPI1_SR.
How is it possible that a receive only SPI with CRC enabled detects no CRC error in this case ?