Nucleo-H563ZI: Blink LED with TrustZone enabled
Hii Sir,
Recently I have got Nucleo-H563ZI nucleo board and i was trying to do programming for blinking led present on the board with the trust zone activated, but i am unable to get how to do it.
The process i follow is;
1) Created new stm32 project -> Give the name of the project -> selected with TrustZone -> Finish. As the onboard LED was already defined in the .ioc file. Therefore generated the project with the default configuration, under main folder, two more folder were generated secure and non-secure. in nonsecure folder -> Core -> Src -> main.c in this main.c file searched for while loop and added toggleing of led code in it and build the code. As there was confusion which code to be uploaded first i tried to upload the nonsecure folder but the led was not blinking (only the led was on ) during this when I press the reset button the led was off. second time, I build the secure folder code and flash it in the microcontroller toggleing was working but the led that was on was off.
2) I followed some youtube tutorial in that in stm32cube ide there was example code, i searched for the GPIO_Toggle code with trustzone for the particular board (STM32H563ZI nucleo) and generated code for it but that was also not working.
I am getting confused and not getting the flow that how write code for this microcontoller as in this I was facing problem with led blinking, consider i want to connect mpu6050 which has i2c protocol for communication how to write code for it like after initializing the pin in ioc file and code generation what steps to be done.
As previously, I was using STM32F407 there was direct coding that due to Trustzone I am getting confused about the flow.
Thankyou,
Regards,
Shubham