Skip to main content
SPati.7
Associate III
April 21, 2022
Solved

PCROP memory protection configuration is not clearing on NUCLEO-H753ZI evaluation board.

  • April 21, 2022
  • 2 replies
  • 1150 views

As per information, PCROP configuration has to be cleared on regression of RDP Level from 1 to 0. But on NUCLE-H753ZI evaluation board, PCROP configuration is not clearing on regression.

0693W00000LybTxQAJ.pngBut it is showing as OPTION BYTES Programming successful.

Can you please help with this, as we locked on this and not able to program application on to this FLASH protected AREA.

@Jocelyn RICARD​  Can you help with this ??

This topic has been closed for replies.
Best answer by Jocelyn RICARD

Hello @SPati.7​ ,

please avoid answering to yourself, as your post will be viewed as already answered.

On STM32H7, you need to change the PCROP range, giving a start address higher than the end address at the same time of the regression from RDP Level 1 to RDP Level 0

Best regards

Jocelyn

2 replies

SPati.7
SPati.7Author
Associate III
April 21, 2022

@Jocelyn RICARD​  Can you please help with this ??

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
April 21, 2022

Hello @SPati.7​ ,

please avoid answering to yourself, as your post will be viewed as already answered.

On STM32H7, you need to change the PCROP range, giving a start address higher than the end address at the same time of the regression from RDP Level 1 to RDP Level 0

Best regards

Jocelyn

SPati.7
SPati.7Author
Associate III
April 22, 2022

Thank You very much @Jocelyn RICARD​, it's working for me now.

Earlier i tried by PCORP config separately and RDP protection level regression separately.