postbuild for OEMiROT project H523
- March 17, 2025
- 1 reply
- 722 views
Hi,
I have managed to extract the OEMiROT project from H533 into H523 and compiled it successfully using STM32CRYPTO library since H523 does only have limited cryptography accelerator. I have modified the flash_layout.h to match my application (which is only using the non-secure image with no data image). However, the OEMiROT bootloader firmware itself is configured with secure and non-secure parts.
I have been updating the postbuild.sh script to match my project structure. I am at the stage or running AppliCfg.exe and it error out on the flash layout with the following error
[ERR] The script was probably invoked manually with having certain macros nested in flash_layouts.h.
Please revisit the flash_layout.h file and hardcode values for the (NON-)SECURE_IMAGE_OFFSET and (NON-)SECURE_IMAGE_MAX_SIZE macros
I checked these macros and they are matching the ones in map.properties. I also tested with
I attached the following files:
1. flash_layout.h
2. map.properties
3. postbuild.log
Kind Regards,
Hani