Problem with SBSFU_STM32L496G-Discovery_Cloud_AWS_V1.4.0.bin (P-L496G-CELL02)
Hi
I am going to use the binary file (SBSFU_STM32L496G-Discovery_Cloud_AWS_V1.4.0.bin) on development kit P-L496G-CELL02 to connect AWS server. However, the boot up prompt message does not include the configuration of external SIM card and VPN entry, so I cannot take the next step to do AWS root certificate update. Please let us know how to config the BG96 modem.Thanks !
Beside, I cannot find project file (.ioc) in STM32CubeExpansion_Cloud_AWS_V1.4 2 folder. It only has (.uvprojx) and (.eww) project files but I don’t have IAR or KEIL compliers to open it. Can I know whether it has any project file that can be opened by STM32cubeMX ?
Regards,
Kelvin.
.
= [SBOOT] System Security Check successfully passed. Starting...
= [FWIMG] Slot #0 @: 8080800 / Slot #1 @: 8014000 / Swap @: 80ec800
======================================================================
= (C) COPYRIGHT 2017 STMicroelectronics =
= =
= Secure Boot and Secure Firmware Update =
======================================================================
= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL
= [SBOOT] STATE: CHECK STATUS ON RESET
. INFO: A Reboot has been triggered by a Hardware reset!
. Consecutive Boot on error counter = 0
. INFO: Last execution detected error was:No error. Success.
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK USER FW STATUS
. A valid FW is installed in the active slot - version: 1
= [SBOOT] STATE: VERIFY USER FW SIGNATURE
= [SBOOT] STATE: EXECUTE USER FIRMWARE
Starting Main Thread...
*************************************************************
*** STM32 IoT Discovery kit for
*** STM32F413/STM32F769/STM32L475/STM32L496 MCU
*** X-CUBE-AWS Cloud Connectivity Demonstration
*** FW version 1.4.0 - 07-June-2019 04:09:58 PM
*************************************************************
*** Board personalization ***
- Network Interface initialized:
- Network Interface starting:
*** C2C connection ***
Initializing the cellular module
- Network Interface connecting:
Trying to connect with the external SIM
Waiting for BG96 modem running
Signal not known or not detectable yet (be patient)
......................
Signal Level: -79 dBm
...........
C2C module registered
Registration done in 30024 msseconds
Retrieving the cellular operator: "3 (2G)"
Module initialized successfully: Quectel
ProductID: BG96
FW version: BG96MAR02A07M1G
SIM Id (IccID): 8985203104047687826F
- Network Interface started:
- Device Name : Quectel.
- Device ID : BG96.
- Device Version : BG96MAR02A07M1G.
Download path: