Question about STM32L562E-DK demo with "TFM application"?
Hi,
I followed document "readme.txt" in "STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM" to family with TFM, it work fine.
My question:
1: "press reset button or restart the board power" will lock the board.
Please tell me what code in the "STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM" cause the board locked, and list the code for me.
2:"Remove JP2 jumper on STM32L562E-DK board, then put it back in place" can unlock the board, but I can't unlock the board via restarting the board power. please explain more detailly for me, or show me what code is used to unlock the board in "STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM".
Thanks,
QiZhang