Skip to main content
DTsai.2
Visitor II
July 27, 2022
Question

question for orientation for IC pin 1 in tape reel on STSAFE-A110.

  • July 27, 2022
  • 1 reply
  • 875 views

STSAFE-A110 series are come in Reel packaging, it's SO-8 package ,I need to know the orientation for IC pin 1 in tape reel. could you hlep to inform us for this question?

    This topic has been closed for replies.

    1 reply

    ST Employee
    October 10, 2022

    Hi @DTsai.2​ 

    The pin 1 is on ST logo side which is on the same side as the sprocket holes in the tape.

    Best Regards,

    Benjamin