Questions about PCROP, Firewall and RDP protections
Hi,
I am using the the SecureBoot on a STM32L4 with the KMS, I have some questions related to the protections:
- As I use the KMS, I read in the UM2262: "With KMS middleware integration, SBSFU keys are no more stored in a section under PCROP protection but inside the KMS code running in the secure enclave". So what is the effect of activating the SFU_PCROP_PROTECT_ENABLE in app_sfu.h ?
- If I don't activate SFU_FWALL_PROTECT_ENABLE, can a malicious user application read the keys from the KMS code running in the secure enclave? If yes, does activating the firewall protection make the secrets from the KMS code running in the secure enclave un-readable by the User App ?
- I read in UM2262 that using RDP L1 is not recommended because WRP can be reprogrammed. So if I understood correctly, a malicious attacker with physical access to the hardware could disable WRP and use a malicious User App to overwrite the keys in the flash. However how could that malicious app be installed as it won't be signed with the correct key (I make the assumption that the attacker does not have the key used to signed the User App)?
Thanks in advance,
Benjamin