Question
RDP level1 is automatically SET on STM32F407 ! STRANGE ISSUE!
Posted on October 16, 2014 at 17:32
Hi all,
I have a very strange issue with STM32F407ZG; sometimesthe RDP level 1 is automatically set and then using STLink Utilities I can goback to RDP level 0.BUT, Now I get RDP level 1 SET and I can't go toRDP level 0 : Seems to be Irreversible (like RDP level2).I can connect with STLink utilities, to read theoption bytes and I see RDP Level1 and I'm not able to modify it to go to RDPlevel 0.Canany one help please ? it is urgent!Thx,Franco #stm32f4 #rdp-level-1