Skip to main content
Associate
October 6, 2025
Solved

Recovering STM32U3 from RDP2 level to RDP1 level

  • October 6, 2025
  • 3 replies
  • 358 views

Hi team,

 

I provisioned both OEM1 and OEM2 keys. I locked the device using OEM2 key and then put the device in RDP level 2 with the below commands:

STM32_Programmer_CLI.exe -c port=SWD mode=hotplug -lockRDP2 0xFEDCBA98 0x76543210

Response: "Lock RDP2 password successfully done"

Enable RDP2: STM32_Programmer_CLI.exe -c port=SWD mode=hotplug -ob RDP=0xCC

If you see here I used only <word1> and <word2> for password because I followed the below video for STM32U5:

URL: https://www.youtube.com/watch?v=B3l6iuA7U8Q&t=752s

But STM32U3 series uses 128 bits of password rather than 64 bits used by STM32U5 series.

Could anyone know/share default value that will be passed if we have missed <word3> and <word4>.

 

 

Best answer by KDJEM.1

Hello @deva2k and welcome to the community;

 

Thank you for bringing this issue to our attention.

The expected behavior that a warning/error message should be displayed when you define two words.

The Bits[64:127] are written as zero so in reality OEM2KEY = 0xFEDCBA98 0x76543210 0X00000000 0X00000000.

 

I reported this issue internally.

 Internal ticket number is reported : 195040 (This is an internal tracking number and is not accessible or usable by customers)

 

Thank you.

Kaouthar

3 replies

KDJEM.1
KDJEM.1Best answer
Technical Moderator
October 6, 2025

Hello @deva2k and welcome to the community;

 

Thank you for bringing this issue to our attention.

The expected behavior that a warning/error message should be displayed when you define two words.

The Bits[64:127] are written as zero so in reality OEM2KEY = 0xFEDCBA98 0x76543210 0X00000000 0X00000000.

 

I reported this issue internally.

 Internal ticket number is reported : 195040 (This is an internal tracking number and is not accessible or usable by customers)

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
deva2kAuthor
Associate
October 15, 2025

Hello @KDJEM.1 

The Bits[64:127] are written as zero so in reality OEM2KEY = 0xFEDCBA98 0x76543210 0X00000000 0X00000000.

The above password worked. Thanks!

Just to clarify, when TrustZone (TZEN) is enabled, you need to set BOOT0 to high by connecting it to 3.3V.

KDJEM.1
Technical Moderator
October 15, 2025

Hello @deva2k ,

 

Glad to know that the issue is solved.

The STM32CubeProgrammer issue is reported under 195040 ticket.

I will let you know when the issue is fixed.

 

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KDJEM.1
Technical Moderator
November 28, 2025

Hello @deva2k;

 

The issue is fixed in STM32CubeProgrammer 2.21.0 version.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.