Replace SBSFU Uart local loader for USB. Crypto in Secure Engine is failing.
Hey guys,
I need to replace Uart for USB on my SBSFU local loader. I manage to create the USB comm in SBSFU quite easily, using UART structure provided in the SBSFU examples. My problem is when i receive firmware header, my code get stuck on the following part in the Secure Engine:
int32_t status;
PKA_ECDSAVerifInTypeDef ECDSA_verif = {0};
const uint8_t *pSign_r;
const uint8_t *pSign_s;
/* Firmware metadata to be authenticated and reference MAC */
const uint8_t *pPayload; /* Metadata payload */
int32_t payloadSize; /* Metadata length to be considered for hash */
uint8_t *pSign; /* Reference MAC (ECCDSA signed SHA256 of the FW metadata) */
const uint8_t *pPub_x;
const uint8_t *pPub_y;
/* buffer for sha256 computing */
uint8_t MessageDigest[CRL_SHA256_SIZE];
int32_t MessageDigestLength = 0;
/* the key to be used for crypto operations (as this is a pointer to m_aSE_FirmwareKey or m_aSE_PubKey it can be a
local variable, the pointed data is protected) */
uint8_t *pKey;This is inside the SE_CRYPTO_Authenticate_Metadata on the Secure Engine (i configured my debugger with SBSFU and SE .elf, so that i could be able to debug both codes). Code goes until line number two of the code snippet above, then after that i see with debug that code keeps looping in this part of startup file:
Reset_Handler:
Infinite_Loop:
b Infinite_Loop
.size Reset_Handler, .-Reset_HandlerThis is the call stack until infinite loop:
Thread #1 [main] 1 [core: 0] (Suspended : Breakpoint)
SE_CRYPTO_Authenticate_Metadata() at se_crypto_bootloader.c:1.064 0x8000bcc
SE_CallGateService() at se_callgate.c:841 0x80023ac
SE_CallGate() at se_callgate.c:311 0x80002b8
SE_VerifyHeaderSignature() at se_interface_bootloader.c:701 0x8003bb8
SFU_LOADER_VerifyFwHeader() at sfu_loader.c:942 0x8005342
SFU_COM_USB_DataPktRxCpltCallback() at sfu_loader.c:733 0x80055e2
SFU_COM_USB_Receive() at sfu_com_loader.c:358 0x8004b4c
SFU_LOADER_DownloadNewUserFw() at sfu_loader.c:135 0x8005516
SFU_BOOT_SM_DownloadNewUserFw() at sfu_boot.c:748 0x80043b2
SFU_BOOT_SM_Run() at sfu_boot.c:416 0x80047a4
<...more frames...> I fell this could be something related to my ram partitioning. Here's how my mapping_sbsfu.ld is:
/* SE Code region */
VECTOR_SIZE = 0x200;
__ICFEDIT_SE_Code_region_ROM_start__ = 0x08000000 + VECTOR_SIZE;
__ICFEDIT_SE_CallGate_region_ROM_start__ = __ICFEDIT_SE_Code_region_ROM_start__; /* No need to do +4 as we have dummy bytes in SE_CoreBin .ld file */
__ICFEDIT_SE_CallGate_region_ROM_end__ = __ICFEDIT_SE_Code_region_ROM_start__ + 0x1FF;
/* SE key region */
__ICFEDIT_SE_Key_region_ROM_start__ = __ICFEDIT_SE_CallGate_region_ROM_end__ + 0x1;
__ICFEDIT_SE_Key_region_ROM_end__ = __ICFEDIT_SE_Key_region_ROM_start__ + 0xFF;
/* SE Startup */
__ICFEDIT_SE_Startup_region_ROM_start__ = __ICFEDIT_SE_Key_region_ROM_end__ + 0x1;
__ICFEDIT_SE_Code_nokey_region_ROM_start__ = __ICFEDIT_SE_Startup_region_ROM_start__ + 0x100;
__ICFEDIT_SE_Code_region_ROM_end__ = __ICFEDIT_SE_Startup_region_ROM_start__ + 0x31FF;
/* SE IF ROM */
__ICFEDIT_SE_IF_region_ROM_start__ = __ICFEDIT_SE_Code_region_ROM_end__ + 1;
__ICFEDIT_SE_IF_region_ROM_end__ = __ICFEDIT_SE_IF_region_ROM_start__ + 0x5FF;
/* SBSFU Code region */
__ICFEDIT_SB_region_ROM_start__ = __ICFEDIT_SE_IF_region_ROM_end__;
__ICFEDIT_SB_region_ROM_end__ = 0x0801FFFF;
/* LOADER code region : 20 kBytes area aligned on 4kBytes address, MPU protection constraints */
__ICFEDIT_LOADER_region_ROM_start__ = __ICFEDIT_SB_region_ROM_end__ + 0x1;
__ICFEDIT_LOADER_region_ROM_end__ = 0x0802FFFF;
SE_Entry_Secure_ROM_Region_Length = __ICFEDIT_SE_CallGate_region_ROM_end__ - __ICFEDIT_SE_CallGate_region_ROM_start__ + 1;
SE_Key_region_ROM_Length = __ICFEDIT_SE_Key_region_ROM_end__ - __ICFEDIT_SE_Key_region_ROM_start__ + 1;
SE_Startup_region_ROM_Length = __ICFEDIT_SE_Code_nokey_region_ROM_start__ - __ICFEDIT_SE_Startup_region_ROM_start__ ;
SE_ROM_region_Length = __ICFEDIT_SE_Code_region_ROM_end__ - __ICFEDIT_SE_Code_nokey_region_ROM_start__ + 1;
SE_IF_region_ROM_Length = __ICFEDIT_SE_IF_region_ROM_end__ - __ICFEDIT_SE_IF_region_ROM_start__ + 1;
SB_ROM_region_Length = __ICFEDIT_SB_region_ROM_end__ - __ICFEDIT_SB_region_ROM_start__ + 1;
LOADER_ROM_region_Length = __ICFEDIT_LOADER_region_ROM_end__ - __ICFEDIT_LOADER_region_ROM_start__ + 1;
/* RAM section */
/* SE stack is placed 1st in RAM, stack overflow does not write on other RAM area */
__ICFEDIT_SE_region_RAM_start__ = 0x20000000;
__ICFEDIT_SE_region_RAM_stack_top__ = 0x20000400;
__ICFEDIT_SE_region_RAM_end__ = 0x20000FFF;
/* LOADER communication region when bypass mode activated */
__ICFEDIT_LOADER_COM_region_RAM_start__ = __ICFEDIT_SE_region_RAM_end__ + 1;
__ICFEDIT_LOADER_COM_region_RAM_end__ = __ICFEDIT_LOADER_COM_region_RAM_start__ + 0x0F;
/* LOADER RAM1 region */
__ICFEDIT_LOADER_region_RAM_start__ = __ICFEDIT_LOADER_COM_region_RAM_end__ + 1;
__ICFEDIT_LOADER_region_RAM_end__ = 0x2002FFFF;
/* SBSFU RAM1 region */
__ICFEDIT_SB_region_RAM_start__ = __ICFEDIT_LOADER_COM_region_RAM_end__ + 1;
__ICFEDIT_SB_region_RAM_end__ = 0x2004FFFF;
SE_RAM_region_Length = __ICFEDIT_SE_region_RAM_end__ - __ICFEDIT_SE_region_RAM_stack_top__ + 1;
LOADER_RAM_region_Length = __ICFEDIT_LOADER_region_RAM_end__ - __ICFEDIT_LOADER_region_RAM_start__ + 1;
SB_RAM_region_Length = __ICFEDIT_SB_region_RAM_end__ - __ICFEDIT_SB_region_RAM_start__ + 1;
MEMORY
{
SE_Entry_Secure_ROM_Region (rx) : ORIGIN = __ICFEDIT_SE_CallGate_region_ROM_start__, LENGTH = SE_Entry_Secure_ROM_Region_Length
SE_Key_region_ROM (rx) : ORIGIN = __ICFEDIT_SE_Key_region_ROM_start__, LENGTH = SE_Key_region_ROM_Length
SE_Startup_region_ROM (rx) : ORIGIN = __ICFEDIT_SE_Startup_region_ROM_start__, LENGTH = SE_Startup_region_ROM_Length
SE_ROM_region (rx) : ORIGIN = __ICFEDIT_SE_Code_nokey_region_ROM_start__, LENGTH = SE_ROM_region_Length
SE_IF_region_ROM (rx) : ORIGIN = __ICFEDIT_SE_IF_region_ROM_start__, LENGTH = SE_IF_region_ROM_Length
SB_ROM_region (rx) : ORIGIN = __ICFEDIT_SB_region_ROM_start__, LENGTH = SB_ROM_region_Length
LOADER_ROM_region (rx) : ORIGIN = __ICFEDIT_LOADER_region_ROM_start__, LENGTH = LOADER_ROM_region_Length
SE_RAM_region (xrw) : ORIGIN = __ICFEDIT_SE_region_RAM_stack_top__, LENGTH = SE_RAM_region_Length
LOADER_RAM_region (xrw) : ORIGIN = __ICFEDIT_LOADER_region_RAM_start__, LENGTH = LOADER_RAM_region_Length
SB_RAM_region (xrw) : ORIGIN = __ICFEDIT_SB_region_RAM_start__, LENGTH = SB_RAM_region_Length
RAM_SHARED (rw) : ORIGIN = 0x20030000, LENGTH = 10K
}I changed the __ICFEDIT_SB_region_RAM_end__ to 0x2004FFFF to see if it would solve anything but the behaviour kept the same.
I also had to alter the SB ROM lenght, since i'm now using USB and the code is bigger.
Hope anyone can help me.
Thanks in advance,
Matheus