SBSFU News ! New SBSFU 2.6.1 release available solving build issue with STM32CubeIDE
Hello,
The new SBSFU 2.6.1 is available now.
The main change concerns the compatibility with latest STM32CubeIDE based on GNU Tools 10.3 which are version 1.9.0 and 1.10.1
There is no need anymore to follow the steps provided previously to have a successful build.
The new SBSFU version 2.6.1 includes the same change that was proposed in this post
Also, it is no more needed to fill the export control form.
SBSFU can now be downloaded like any other package on st.com !
Enjoy :grinning_face:
Best regards
Jocelyn