Skip to main content
RAbd.1
Visitor II
March 12, 2020
Question

SBSFU project Failed to build UserApp

  • March 12, 2020
  • 3 replies
  • 1108 views

I am trying to build SBSFU V2.3.0 on STM32L496G-DISCOVERY board. I can build SeCoreBin and SBSFU. Flashed into board. All fine and it comes up over serial usb. However I am having trouble building the user app to exercise flashing. I am building on system workbench.

The build is fine but it fails running the post build scripts:

Building target: UserApp.elf

Invoking: MCU GCC Linker

arm-none-eabi-gcc -z max-page-size=8 -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -L"/ml/Users/MAGICLEAP/rabd/Downloads/STM32CubeExpansion_SBSFU_V2.3.0/Projects/32L496GDISCOVERY/Applications/2_Images/2_Images_SBSFU/SW4STM32/STM32L496G-Discovery_2_Images_SBSFU/Debug" -specs=nosys.specs -specs=nano.specs -Xlinker -L ../../../../Linker_Common/SW4STM32 -T"../STM32L496AGIx_FLASH.ld" -Wl,-Map=output.map -Wl,--gc-sections -o "UserApp.elf" @"objects.list" -l:se_interface_app.o -lm

Finished building target: UserApp.elf

make --no-print-directory post-build

Generating binary and Printing size information:

arm-none-eabi-objcopy -O binary "UserApp.elf" "../../UserApp.bin"

arm-none-eabi-size "UserApp.elf"

  text   data   bss   dec   hex filename

 27488   368   5288  33144   8178 UserApp.elf

"../../../../2_Images_SECoreBin/SW4STM32/postbuild.sh" "../.." "./UserApp.elf" "../../UserApp.bin" "1"

/bin/bash: - : invalid option

Usage: /bin/bash [GNU long option] [option] ...

/bin/bash [GNU long option] [option] script-file ...

makefile:53: recipe for target 'post-build' failed

GNU long options:

makefile:40: recipe for target 'UserApp.elf' failed

--debug

--debugger

--dump-po-strings

--dump-strings

--help

--init-file

--login

--noediting

--noprofile

--norc

--posix

--rcfile

--restricted

--verbose

--version

Shell options:

-ilrsD or -c command or -O shopt_option (invocation only)

-abefhkmnptuvxBCHP or -o option

make[1]: *** [post-build] Error 2

make: *** [UserApp.elf] Error 2

12:08:18 Build Finished (took 11s.774ms)

Any idea?

Thank you

This topic has been closed for replies.

3 replies

Arno1
Senior
March 12, 2020

Hi,

Can you try doing this from a terminal?

cd WHERE/YOU/PUT/THE/PACKAGE/2_Images_SECoreBin/SW4STM32/
dos2unix *.sh

Let us know if it worked!

Cheers,

Arno

Skuma.6
Associate II
September 4, 2020

Hi

Im also facing same issue while compiling UserApp project. Below is the error and it also shows on postbuild.sh . I haven't done any changes to the code just wanted to run as is. Im using STM32H7B3i-DK , and STM32CubeIDE on windows.

"../../../../2_Images_SECoreBin/STM32CubeIDE/postbuild.sh" "../.." "./UserApp.elf" "../../UserApp.bin" "1"

prepareimage with windows executeable

[11544] Failed to execute script prepareimage

Traceback (most recent call last):

 File "prepareimage.py", line 759, in <module>

 File "prepareimage.py", line 756, in args

 File "prepareimage.py", line 123, in do_encrypt

 File "keys.py", line 262, in load

FileNotFoundError: [Errno 2] No such file or directory: '../../../../2_Images_SECoreBin/STM32CubeIDE/../Binary/OEM_KEY_COMPANY1_key_AES_CBC.bin'

../../../../2_Images_SECoreBin/STM32CubeIDE/postbuild.sh: line 68: prepareimage.exe: No error

prepareimage.exe enc -k ../../../../2_Images_SECoreBin/STM32CubeIDE/../Binary/OEM_KEY_COMPANY1_key_AES_CBC.bin -i ../../../../2_Images_SECoreBin/STM32CubeIDE/../Binary/iv.bin ../../UserApp.bin ../../../Binary/UserApp.sfu : failed

make[1]: *** [makefile:85: post-build] Error 1

make: *** [makefile:51: all] Error 2

"make all" terminated with exit code 2. Build might be incomplete.

Skuma.6
Associate II
September 7, 2020

Hi

I expanding the zip file of STM32CubeExpansion_SBSFU_V2.3.0 in C:\ and compiled all the project folders and also could build UserApp.

thanks