SBSFU-UserApplication-Debugging
I'm curious what is the best way to debug a User Application when using SBSFU on a STM32.
Of course the security mechanisms in SBSFU/SECore must be disabled to allow debugging at all and basically just downloading the UserApplication and debug it with e.g. CubeIDE works as the programmer manipulates the PC to start in the application. But the problem is once the application resets (e.g. SW-Reset) it reboots over the Secure Boot and deletes the application as it was not installed correctly via the SFU. This becomes very tricky in case of debugging something that happens on startup!?
I know that flashing the FW via SFU and then only attaching the Debugger is a working option but it becomes plumby if doing repeated code-changes to the application.
Is there any other suggested way to do that?