Secure Boot and Secure Update Software Options
Hi, I'm building a medical device that will use an STM32 MCU and requires secure boot and secure firmware updates (over USB-C preferably). I have little experience with implementing secure bootloaders, and am looking for a solution that could allow me to get secure boot working out-of-the-box with minimal setup. I've seen that SBSFU offers example projects for secure boot on some MCUs, while MCUboot is also available for some others. It also looks like the STM32U5 series supports their own secure firmware updates based on AN4992. What's the difference between all of these solutions? Out of all the solutions ST offers for secure boot, which ones are the newest/recommended and easiest to get set up with? Because I'm looking for a low-cost MCU, I've identified the STM32L471, STM32L476, and STM32U575 as potential candidates that could support secure boot, but I'm lost as to how to actually set it up or what software solution to use. I'd love to hear anyone else's suggestions for other MCUs I could use that easily support these security features, or for application notes/resources I could use to learn how to use ST's security solutions.