Skip to main content
Associate II
June 23, 2025
Question

SFI programm STM32L562 do not work.

  • June 23, 2025
  • 3 replies
  • 491 views

Good day!

I have custom board with cpu stm32l562. I am prepared all data and global license. 

CPU prepared by script file from package STM32CubeExpansion_SFI_v1.5.0 L5.

This operation is OK.

But after if start programm by Cube Programmer ( v 2.19 ) - i have error all times.

I am add log with this errors...

Help me, please.

 

12:25:13 : SFI parsing file started ...
12:25:13 : SFI header information :
12:25:13 : SFI protocol version : 2
12:25:13 : SFI total number of areas : 4
12:25:13 : SFI image version : 0
12:25:13 : SFI Areas information :
12:25:13 : Parsing Area 1/4 :
12:25:13 : Area type : F
12:25:13 : Area size : 80560
12:25:13 : Area destination address : 0x8040000
12:25:13 : Parsing Area 2/4 :
12:25:13 : Area type : F
12:25:13 : Area size : 65664
12:25:13 : Area destination address : 0xC000000
12:25:13 : Parsing Area 3/4 :
12:25:13 : Area type : F
12:25:13 : Area size : 128
12:25:13 : Area destination address : 0xC03E000
12:25:13 : Parsing Area 4/4 :
12:25:13 : Area type : C
12:25:13 : Area size : 48
12:25:13 : Area destination address : 0x0
12:25:13 : Parsed File SUCCESS
12:25:29 : Starting Firmware Install operation...
12:25:30 : Warning: Option Byte: TZEN, value: 0x1, was not modified.
12:25:31 : Reconnecting...
12:25:32 : Reconnected !
12:25:32 : Time elapsed during option Bytes configuration: 00:00:02.160
12:25:32 : Warning: Option Byte: SECWM1_PEND, value: 0x7F, was not modified.
12:25:32 : Warning: Option Byte: SECWM1_PSTRT, value: 0x0, was not modified.
12:25:32 : Warning: Option Bytes are unchanged, Data won't be downloaded
12:25:32 : Time elapsed during option Bytes configuration: 00:00:00.005
12:25:33 : Reconnecting...
12:25:34 : Reconnected !
12:25:34 : Time elapsed during option Bytes configuration: 00:00:02.161
12:25:34 : Warning: Option Byte: SECBOOTADD0, value: 0x1FF000, was not modified.
12:25:34 : Warning: Option Bytes are unchanged, Data won't be downloaded
12:25:34 : Time elapsed during option Bytes configuration: 00:00:00.006
12:25:34 : Installing RSSe
12:25:34 : Opening and parsing file: RSSe_SFI_L552_L562_v6.0.0.bin
12:25:34 : Memory Programming ...
12:25:34 : File : RSSe_SFI_L552_L562_v6.0.0.bin
12:25:34 : Size : 35.92 KB
12:25:34 : Address : 0x20005100
12:25:34 : Erasing memory corresponding to sector 0:
12:25:34 : Download in Progress:
12:25:34 : File download complete
12:25:34 : Time elapsed during download operation: 00:00:00.078
12:25:34 : Warning: Option Byte: TZEN, value: 0x1, was not modified.
12:25:34 : Warning: Option Byte: nBoot0, value: 0x0, was not modified.
12:25:34 : Warning: Option Byte: nSWBoot0, value: 0x0, was not modified.
12:25:34 : Warning: Option Bytes are unchanged, Data won't be downloaded
12:25:34 : Time elapsed during option Bytes configuration: 00:00:00.006
12:25:34 : Error: Execution of RSS CMD failed, returned value = 0x20005014
12:25:34 : Error: Installing the RSSe failed!
12:25:35 : Error: Cannot launch RSSe...

3 replies

dlpPavloAuthor
Associate II
June 24, 2025

Small add. I am using SFIG ( global license ). 

Frantz LEFRERE
ST Employee
June 24, 2025

@dlpPavlo,

if the SFIG ( global license ), you are refering to the mechanism describe in this wiki page :
https://wiki.st.com/stm32mcu/wiki/Security:SFI_for_STM32H5#SFI_for_STM32H5_without_Secure_Manager
"
The OEM provisions its OEM key, using the Trusted Package Creator, in one global license file."
This mechanism is available only on STM32H5 and with the Secure Manager.

dlpPavloAuthor
Associate II
June 24, 2025

Thank you for response! I will order card and work with it. The  question is how  can I return CPU to default state? I used to run debug in stm32cubeide before my changes. But I can't after i have enabled TZEN. Are those changes revertable at all?

Best regards.  

Frantz LEFRERE
ST Employee
June 24, 2025

@dlpPavlo 
 To disable TZ,  it should be associated with a RDP regression.
Please have a look in this video :
https://www.youtube.com/watch?v=4UW8lnbV1cA&list=PLnMKNibPkDnGxKqGyLbiGygmlrvISIBIT&index=2

Best regards,

Frantz 

dlpPavloAuthor
Associate II
June 24, 2025

Yes, i can disable TZ. But on next my boards I can debug with TZ enable. This board work the same before my test write SFI. Now if I set TZ - debug not started only on this board...