Skip to main content
This topic has been closed for replies.
Best answer by BRusl.1

Figured out the problem - the STM32C0116-DK when connected to USB must not be opened by any host app or MCU will detect onboard programmer and hard faults. My shame ;)

5 replies

BRusl.1
BRusl.1Author
Associate II
February 21, 2023

Hi,

  

[ ... deleted... ]

Issue is that STLink must not be opened by any host app, see below

BRusl.1
BRusl.1Author
Associate II
February 22, 2023

I'm having two STM32C0116-DK boards. So I've made the simple experiment, unpacked the second board that is shipped with _stock_ LED blinking project and locked it to RDP 1 with :

STM32_Programmer_CLI -c port=SWD freq=4000 -ob RDP=0xBB

Repowered it and guess what ? It stopped blinking exactly as my simple project above. I guess there is real problem with STM32C0 series concerning this issue.

BRusl.1
BRusl.1Author
Associate II
February 22, 2023

Made the same experiment with STM32C0316-DK and all is working as expected - RDP 1 do not crash the firmware. Seems like problem is related at least to STM32C0116

Simon.T
ST Employee
February 22, 2023

Hello @BRusl.1​ ,

I did the test with the C011DK, C031DK and NUCLEO, I never observed the issue. I changes the RDP with cube programmer and then after a POR the LED MCU is working fine (LED blinking with HAL delay of 100ms).

Which product revision are you using ? And did you do the POR after changing the RDP ?

BR,

Simon

BRusl.1
BRusl.1AuthorBest answer
Associate II
February 22, 2023

Figured out the problem - the STM32C0116-DK when connected to USB must not be opened by any host app or MCU will detect onboard programmer and hard faults. My shame ;)

Peter BENSCH
Technical Moderator
February 22, 2023

Mistakes are there to be learned from. ;)

Thank you for finding this and reporting it back here!

Regards

/Peter