STM32CubeU5 TFM swap strategy, secure loader
Hello,
I am working with STM32CubeU5 TFM v1.5 for STM32 u585. I develop a custom loader using CAN communication. First I used MCUBOOT_OVERWRITE_ONLY and MCUBOOT_PRIMARY_ONLY setup. The CAN communication worked fine (in non-secure loader).
Then I switched to swap strategy (MCUBOOT_OVERWRITE_ONLY and MCUBOOT_PRIMARY_ONLY not defined). The CAN communication stopped working. After quite some investigation I found out that the reason is that the FDCAN IRQ is not enabled (although set to be enabled). Then I found out that the reason is probably due to the FDCAN1_IT0_IRQn is not set in ITNS1 for the non-secure domain. This can be handled in the secure loader.
Unfortunately, in this mode the secure loader is not used. I am not sure why, did I misconfigure or misunderstand something?
Any advise how to get interrupt enabled in the the non-secure loader in this mode?
Thanx.
Best regards,
peter