STM32CubeWL SBSFU compile error on Windows
Hi there,
I am trying to compile the SBSFU_2_Images_DualCore project.
Although I did it in the correct order according to the document "Getting started with the SBSFU of STM32CubeWL (UM2767)". I am getting a compiler error.
I'm sure that, compiling the correct order according to Getting started with the SBSFU of STM32CubeWL (UM2767)
Compile order is;
- 2_Images_SECoreBin - compile success
- 2_Images_KMS_Blob - compile success
- 2_Images_SBSFU
- 2_Images_SBSFU_CM0PLUS - compile success
- 2_Images_SBSFU_CM4) - compile success
- 2_Images_UserApp_CM4 - compile success
- 2_Images_UserApp_CM0PLUS - compiler error
The error is multiple definition error .
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o: in function `SE_KMS_CloseSession':
(.SE_IF_Code+0xbd8): multiple definition of `SE_KMS_CloseSession'; ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o:(.SE_IF_Code+0xbd8): first defined here
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o: in function `SE_KMS_DigestInit':
(.SE_IF_Code+0x121c): multiple definition of `SE_KMS_DigestInit'; ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o:(.SE_IF_Code+0x121c): first defined here
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o: in function `SE_KMS_EncryptInit':
(.SE_IF_Code+0xedc): multiple definition of `SE_KMS_EncryptInit'; ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o:(.SE_IF_Code+0xedc): first defined here
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o: in function `SE_KMS_DestroyObject':
(.SE_IF_Code+0xc94): multiple definition of `SE_KMS_DestroyObject'; ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o:(.SE_IF_Code+0xc94): first defined here
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o: in function `SE_KMS_Encrypt':
(.SE_IF_Code+0xf3c): multiple definition of `SE_KMS_Encrypt'; ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o:(.SE_IF_Code+0xf3c): first defined here
I didn't do any code change, I just downloaded and opened in STM32CubeIde.
Is this related with STM32Cube_FW_WL_V1.0.0 ?
What's wrong ?
Thank you