STM32CubeWL SBSFU doesn't upload the UserApp.sfb using Linux minicom
Hello,
I am trying to upload the user firmware using BFU(1 slot) and Linux minicom, it always failed to complete to transfer a UserApp.sfu. I have read the UM2767 and followed all steps. But it works well on Windows Tera Term.
I am testing on both of Nucleo55 eval board and custom board and using STM32Cube_FW_WL_V1.0.0(SBSFU version 2.4.0), not succeed.
I have looked for the similar issues, couldn't get the workaround.
There are some similar issues:
https://community.st.com/s/question/0D53W00000Eba1XSAR/download-firmware-by-ymodem-failed-at-linux
Last article tells me this issue would be fixed in SBSFU v2.4.0, but I am failing.
This is what I've done:
- defined MINICOM_YMODEM in app_sfu.h
- Erase flash and upload the BFU.bin
- set minicom 115200bps, 8N1, HW flow control: None.
- ymodem protocol setting:
+------------------------------------------------------------------------------+
| Name Program Name U/D FullScr IO-Red. Multi |
| A zmodem /usr/bin/sz -vv -b Y U N Y Y |
| B ymodem /usr/bin/sb -vv Y U N Y Y |
| C xmodem /usr/bin/sx -vv Y U N Y N |
| D zmodem /usr/bin/rz -vv -b -E N D N Y Y |
| E ymodem /usr/bin/rb -vv N D N Y Y |
| F xmodem /usr/bin/rx -vv Y D N Y N |
| G kermit /usr/bin/kermit -i -l %l -b %b Y U Y N N |
| H kermit /usr/bin/kermit -i -l %l -b %b N D Y N N |
| I ascii /usr/bin/ascii-xfr -dsv Y U N Y N |
It's my minicom log.
Welcome to minicom 2.7.1
OPTIONS: I18n
Compiled on Aug 13 2017, 15:25:34.
Port /dev/ttyUSB0, 21:32:12
+-----------[ymodem upload - Press CTRL-C to quit]------------+
Press CTR|Sending: UserApp.sfb |
|Ymodem sectors/kbytes sent: 191/23kRetry 0: Cancelled |
CC | |
|Transfer incomplete |
| |
| READY: press any key to continue... |
| |
+-------------------------------------------------------------+But the image size is about 24.5kB. :(
Does anyone have any idea?
Any suggestions would be appreciated.
Thanks.