STM32F777 - CRYP Coprocessor not setting the key
Hello,
I'm currently using an STM32F777 MCU with the Keil MDK. I want to run an HTTPS serer on this system, and I set up mbedTLS with Keil's network component (using the TLS_ECDHE_ECDSA_AESGCM128 cipher suite). By default, it takes around 6 seconds for a resource to load, so I tried adding in hardware acceleration using the CRYP coprocessor in the STM32F7. However, I ran into some issues with it.
AES GCM did not work, and when debugging my code it looked as though the AES key registers (CRYP_Kx{L/R}R) were not being set. Any time I would try to set them, the registers would report back that they were 0x00. Should I be able to see these registers set to the key that I am using, or are these blind registers? If they are blind registers, is there another way to verify that the AES key is being properly set in the CRYP processor?
Any help would be appreciated.
Thanks,
Brandon