STM32H563 Debug Authentication Failure with OEMiRoT and product state PROVISIONED
I'm using the link below to select boot path and do secure boot device provisioning for my STM32H563 board:
Boot path is configured as follows:

I have run provisioning.bat, the product state was set to PROVISIONED. The provisioning was successfull, with logs at the end of ob_flash_programming.log:
OPTION BYTE PROGRAMMING VERIFICATION:
Option Bytes successfully programmed
Time elapsed during option Bytes configuration: 00:00:01.334
Programming success
However, inside ob_flash_programming.log, it also shows:
PROGRAMMING OPTION BYTES AREA ...
Warning: Option Byte: boot_ube, value: 0xB4, was not modified.
Warning: Option Byte: hdp2_end, value: 0x0, was not modified.
Warning: Option Byte: secbootadd, value: 0xC0000, was not modified.
Warning: Option Byte: secwm2_end, value: 0x0, was not modified.
Warning: Option Byte: sram2_ecc, value: 0x0, was not modified.
Warning: Option Byte: sram2_rst, value: 0x0, was not modified.
Warning: Option Byte: sram3_ecc, value: 0x1, was not modified.
Warning: Option Byte: swap_bank, value: 0x0, was not modified.
Warning: Option Byte: wrpsgn2, value: 0xFFFFFFFF, was not modified.
Could this indicates that some of the option bytes (e.g., secbootadd) may not be successfully written to flash?
Below is the Option Bytes overview after provisioning:

Everything looks ok, but SECBOOTADD = 0x00000000, it should be 0xC000000 when TZEN = 1 and UBE = B4 (OEMiRoT). Could this be the reason that I can't do Debug Authentication discover and perform DA correctly?

While doing Debug Authentication Discover, it shows error as above image: The target is unable to boot on RSS_DA or is in OPEN mode. Will Debug Authentication requries RSS_DA access which needs to start from SECBOOTADD at 0xC000000?
If so, is there any way to open debug and recover this board at this stage?
Running regression.bat also failed now. It shows a similar error as doing Debug Authentication above:
Start Debug Authentication Sequence
Open SDM Lib
SDMOpen : 624 : open : SDM API v1.0
SDMOpen : 625 : open : SDM Library version v1.2.0
open_comms : 513 : open : Asserting target reset
open_comms : 517 : open : Writing magic number
open_comms : 537 : open : De-asserting target reset
open_comms : 573 : open : No response from the target
open_comms : 574 : open : The target is unable to boot on RSS_DA or is in OPEN mode
open_comms : 575 : open : Failed to open communication with the target
Error:
Debug Authentication Failed
"regression script failed"