STM32H745 configure RDP levels over Lauterbach TRACE32 debugger
Hello,
I am working with the STM32H745 using a Lauterbach TRACE32 debugger and i am evaluating ways to control Readout Protection (RDP).
I am able to configure RDP levels using STM32CubeProgrammer, however I would like to achieve the same using a TRACE32 (.cmm) script, without relying on the ST programmer.
-
Is there any recommended or reference TRACE32 PRACTICE (.cmm) script for setting and reverting RDP levels (Level‑0 to Level‑1) and (Level‑1 to Level‑0) on STM32H7 devices? I could not find any official examples demonstrating direct RDP control using .cmm script.
-
Is it supported or recommended to control RDP level changes from firmware on STM32H745? While setting RDP from Level‑0 to Level‑1 is possible, reverting from Level‑1 to Level‑0 results in a mass erase.
-
When reverting RDP from Level‑1 to Level‑0, is the mass erase automatically triggered by the hardware as part of the RDP regression, or is there an additional register or command that must be explicitly programmed to initiate the mass erase?
Thank you.