STM32U585 / B-U585I-IOT02A: Can't enable GPIOI via RCC_AHB2ENR1
Hello,
I am trying to access the MX25LM NOR-Flash chip on the B-U585I-IOT02A board via OCTOSPI2. The nCS pin is connected to PI5. However, attempting to enabe the peripheral clock for IO port I by setting Bit 8 (GPIOIEN) of register RCC_AHB2ENR1 fails (I.e. bit 8 remains at value 0). For all other IO ports (A-H) it works as expected.
Any idea what might cause this behaviour?
Note: The code is running as a device driver under the Apache NuttX RTOS in the non-secure world. TrustedFirmware-M (from STM32CubeU5 v1.0.2) is running on the secure side.
Any help is very appreciated.
Bye,
Michael