STMU385 - OEMiROT_Appli_TrustZone example - building as combined secure + non-secure doesn't work.
I'm working with the STM32U385/375 for a project, and have started my investigation into how to convert it to a secure root of trust application by working with the OEMiROT examples.
In stock form it works well. The provisioning works, the update over the y-modem link works just fine, etc. However, I want to build a combined binary and not deal with separate non-secure and secure binaries to apply for an update.
Accordingly, I changed MCUBOOT_APP_IMAGE_NUMBER in OEMiROT_Boot/Inc/flash_layout.h from 2 to 1, like so:
#define MCUBOOT_APP_IMAGE_NUMBER 1 /* 1: S application only if FLASH_NS_PARTITION_SIZE = 0 ,
else S and NS application binaries assembled in one single image.
2: Two separated images for S and NS application binaries. */The build works fine, the first part of the provisioning script works fine, the appropriate value is updated in appli_flash_layout.h, and the programming begins. However, it fails with this error:
=====
===== Error while executing "Programming the option bytes and flashing the images...".
===== See "ob_flash_programming.log" for details. Then try again.
=====
I looked in the log, where I see this:
"Application images programming in download slots"
Set boot address @0x1800C0
-------------------------------------------------------------------
STM32CubeProgrammer v2.21.0
-------------------------------------------------------------------
ST-LINK SN : 003C003D3333511631363730
ST-LINK FW : V3J16M7
Board : NUCLEO-U385RG-Q
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x454
Revision ID : Rev Z
Device name : STM32U3xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M33
BL Version : --
Debug in Low Power mode enabled
-------------------------------------------------------------------
Choose flashing speed for Cortex M33 series.(default speed=Reliable)
-------------------------------------------------------------------
Error: File does not exist: oemirot_tz_app_init_sign.bin
I looked in the file system and I don't see that file. I don't see in the provisioning script where it ought to be generated. Any ideas what's going on here and how to fix it?