Stuck in Provisioning State (0x17) - Cannot connect via SWD, USB DFU, or UART
Hello STM32 Community,
I am stuck in a critical situation with my STM32H533RE custom board and need help recovering it. I have exhausted all methods I know.
- Hardware Setup:
- MCU: STM32H533RE (custom PCB, not Nucleo)
- ST-LINK: External ST-LINK V2 (Firmware V2J46S7)
- BOOT0: carry out the cia test point
- USB: DP/DM routed to test points (wires soldered for access)
- SWD: SWCLK , SWDIO , NRST (Pin 2) connected to programming header
- TrustZone Configuration
- Configured Secure and Non-Secure world using STM32CubeMX
- Secure peripherals: SPI1, SPI3, UART4, ICache, DCache
- Flash watermarks configured for secure/non-secure regions
- What Happened (Step by Step)
1. Device was originally in **Open state (0xED)** — everything worked fine
2. I could connect via SWD in Normal mode and read all memory including secure regions
3. I attempted to transition Product State from **Open (0xED) → TZ-Closed (0xC6)** via STM32CubeProgrammer Option Bytes tab
4. The device transitioned to **Provisioning (0x17)** and stopped there (the two-step transition Open→Provisioning→TZ-Closed did not complete)
5. After this, Normal SWD connection stopped working
6. I was able to connect using **Hot Plug mode, Access Port 1, SWD** and confirmed: - Product State = 0x17 (Provisioning) - Device detected as STM32H533/523, 512KB, Cortex-M33 ## Attempted Recovery — All Failed
Attempt 1: OB regression via GUI (Hot Plug, AP1) Changed PRODUCT_STATE from 17 → ED (Open) in Option Bytes tab and clicked Apply.
Error: Expected value for Option Byte "PRODUCT_STATE": 0xED, found: 0x17 Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
Attempt 2: Forward transition 17 → C6
Attempted to complete the transition by setting PRODUCT_STATE to 0xC6.
Result: Connection lost after this attempt. Device no longer connects.
Attempt 3: Mass Erase
- Tried mass erase via ST-M32CubeProgrammer.
Error: Mass erase operation failed. Please verify flash protection
Attempt 4: Under Reset mode
- Connected BOOT0 to VDD (3.3V) via jumper
- Pressed RESET / power cycled the board
- SWD: Tried all combinations (Normal/HotPlug/UnderReset × AP0/AP1 × Freq 100/4000) : None connect
- USB DFU: Connected USB DP/DM to host PC : Windows does not detect any new USB device. No "STM32 BOOTLOADER" or "DFU device" appears in Device Manager
- UART: Connected TTL UART adapter to USART1 (PA9/PA10) : CubeProgrammer UART mode does not connect
- Used a completely different ST-LINK probe.
Result: Same errors. Cannot connect.
Attempt 7: Debug Authentication (DA)
- In Secure Programming section, When click on discover button
Error: Failed to communicate with target
Current State:
- Product State:*0x17 (Provisioning) - or possibly changed during failed attempts
- SWD: Cannot connect in ANY mode (Normal, Hot Plug, Under Reset) with ANY Access Port (0 or 1)
- USB DFU: Not detected by host PC even with BOOT0 confirmed HIGH
- UART Bootloader: Not responsive
- ST-LINK: Detected by Windows, shows serial number and voltage (3.29V) in CubeProgrammer
- Board: Powered correctly (3.3V confirmed)
Error: Cannot connect to access port 1 (or 0)! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.
Questions:
4. Can we goes back to "open mode" from any other mode like provisioning, TZ-closed? or is it reversible?
Any help would be greatly appreciated. This is a custom board for a production project and I need to recover this device if possible.