Suggestions about security?
Hello,
I'm working for an MNC and we use stm32l431cc.
And I have to implement firmware updates over the air.
physical connection:
TARGET DEVICE <---UART----> External IOT DEVICE (GSM MODULE) which can be plugged in and out <----> Cloud service.
For the security part, I need advice or suggestions. I'm new to this topic, so I found confidentiality, integrity, and Authentication are important criteria for this situation.
What I understood confidentiality: No one can decrypt my firmware even if they got this through (physical wire etc.) or through cloud.
Integrity: Know if the firmware is changed or corrupted, intentionally or not. Like a crc check.
Authenticity: A math formula that "I know that this firmware is 100% from this person and decide what to do now".
Question:
integrity and authenticity are quite important. But why confidentiality?? Should I encrypt my software? Because a binary image is just bits right? either 0 or 1?
Can you suggest/advice what is important and what is not?
Also you can suggest where can I insert my CIA in the above physical system? For example using a secure UART or encrypted binary etc. Which is a good option in your opinion?
Question:
Can you also suggest what hardware and software changes to implement this setup?
Note: In this system, everything happens in the background. The consumer cannot know anything. there is no display, only one lead that's all.
Regards,
Vijay