The MCU (STM32G030J6) doesn't execute the code sometimes when RDP level is set to 1.
I am working on STM32G030J6, and I programmed it using STMCubeProgrammer through BOOT0 pin. I have also changed the option bytes nboot_sel to 0 to boot from pin and NRST mode to GPIO. The code works fine when RDP level is set to 0. When RDP is set to 1, the MCU works randomly; it sometimes executes the code and sometimes doesn't. I was wondering if the problem is a hardware problem or a configuration mistake.
Would highly appreciate your help and suggestions.