Unable to import latest TFM app for B-U585I-IOTO2A using MacOS Ventura 13.5,1
I am unable to import the TFM app for the B-U585I-IOTO2A board using MacOS Ventura 13.5.1. Every time I attempt it the importer takes a long time, then fails with a 'Fail on internal error' message. I am using the Import STM32Cube Example method of importing.
In order to fix the problem I have done the following:
1. Deleted and reinstalled STM32CubeIDE 1.13.1
2. Deleted and reinstalled the U5 library version 1.3.0
3. Rebooted the MacBook computer
These did not help at all.
I have successfully installed the 3 required TFM projects for the STM32L562E-DK board. Those three projects installed in just a few seconds.
It seems there is something wrong with the U5 TFM project.
If I can provide further information, please let me know.