Undefined Reference HAL_CRC_Init Function
I want to implement a system so that it retrieves sound by mems microphones and classify it with convolutional neural network. I have spent a lot of times to use BSP Library in my project but I failed. Therefore, I decided to use the code provided in f7cube file in the repository to retrieve sound. Furthermore, I'd like to use xcubeai with this code. To do that, I have to add CRC configuration, however, it throws an error as in the title.
Actually I think this is about linker issue because when I add stm32f7xx_hal_crc.c file to the project, and when I apply ctrl+left click to HAL_CRC_Init in main.c file, it takes me to definition, but cubeide somehow cannot recognize it. How to solve this issue?