Where's the CRC and the size of the whole firmware application stored whenever a new application is flashed on to the System flash?
Does the controller perform a CRC confirmation check before running the application to check if the firmware is corrupted? If so, where does this happen; in the bootloader or the application itself? What does it do if the CRC turns out to be wrong? Secondly, I've referred the AN3155 and in that the bootloader expects a packet size to be a multiple of 4 while issuing the Write memory command (2nd note below the Write Memory Command flow on Pg. 19 of AN3155). So what if the overall firmware size is not a multiple of 4? How to handle the last firmware packet transaction?