Skip to main content
ali rostami
Associate III
October 15, 2022
Solved

Why does DTCM RAM is excluded from the example "2_Images_OSC" of STM32f769I-Discovery?

  • October 15, 2022
  • 1 reply
  • 738 views

Referring to "mapping_sbsfu.h" file of the example "2_Images_OSC" of STM32f769I-Discovery, seems the DTCM and SRAM2 are not used in the project.

So does it have a reason?

This topic has been closed for replies.
Best answer by Fred

Hi @ali rostami​ ,

with X-CUBE-SBSFU, we try not using resources we do not need.

As there is no real need for the bootloader to use the DTCM RAM, we do not use it.

Same reasoning for SRAM2.

Basically, we privilege SRAM1 because on the L0/L4 platforms, this is where the Firewall can be used to provide isolation.

On STM32F769, the isolation is implemented with MPU, but we kept SRAM1 for "consistency reasons".

But, on STM32F7, the main point to observe is the way the MPU regions are configured.

I did not check right now, but in principle, the DTCM is mapped so you can use it in your application.

At bootloader stage, it should be mapped but with instructions disabled.

1 reply

Fred
FredBest answer
ST Employee
October 17, 2022

Hi @ali rostami​ ,

with X-CUBE-SBSFU, we try not using resources we do not need.

As there is no real need for the bootloader to use the DTCM RAM, we do not use it.

Same reasoning for SRAM2.

Basically, we privilege SRAM1 because on the L0/L4 platforms, this is where the Firewall can be used to provide isolation.

On STM32F769, the isolation is implemented with MPU, but we kept SRAM1 for "consistency reasons".

But, on STM32F7, the main point to observe is the way the MPU regions are configured.

I did not check right now, but in principle, the DTCM is mapped so you can use it in your application.

At bootloader stage, it should be mapped but with instructions disabled.