Wrong CRC-32 — HAL_CRC_Calculate output on STM32F401CCU6 Blackpill
I've been implementing I2C communication between F401CCU6 and Nucleo F746ZG, while adding CRC I got different outputs, Nucleo provides configurable CRC peripheral, while F401 is by default set to 0x4C11DB7 (https://www.st.com/resource/en/reference_manual/rm0368-stm32f401xbc-and-stm32f401xde-advanced-armbased-32bit-mcus-stmicroelectronics.pdf#page=68&zoom=100,89,116)
It also provides reseting initial value to 0xFFFF FFFF, ("The CRC calculator can be reset to 0xFFFF FFFF with the RESET control bit in the CRC_CR register. This operation does not affect the contents of the CRC_IDR register")
I've set Nucleo CRC polynomial, init value to match those on BlackPill. Calculated value matches with CRC-32/MPEG-2 standard (available at https://crccalc.com/ for example).
Did anyone has experienced this too?