X-CUBE-SBSFU: Can you use non-secure boot? Also, can you update firmware using USART DFU?
Hello everyone,
I have pretty uncommon question. I'm working on STM32WB with SBSFU, and I'm wondering, if it's possible to use non-secure boot with it? As far as I'm concerned, secure boot is enabled by default, but many security features can be disable using flags.
Also, another question: All the provided examples are using USART YMODEM to transfer data. I know, that it really doesn't matter what kind of protocol you use as long as image is placed in a correct place in the memory, but I wonder if I can use DFU feature to update firmware and still use SBSFU. I think it should be possible.
Thank you in advance.