32F469IDISCOVERY Display Freeze, Touchpanel issue
Hi all,
we're facing some issues with the STM32F469IDISCOVERY board. Sometimes the display seems to be freezing. I started a debug session yesterday and found out that during this error the ft6x06_TS_GetXY function gets called without touching the display. If the error doesn't occur we can see that the ft6x06_TS_DetectTouch function is called frequently to poll for new touch events, right? Only if there is an event the GetXY function is called to get the proper coodinates for the touch event.
This is why I think that during the error state multiple touch events get rocognized without a real touch event.
Our STM32F469IDISCOVERY board uses the FT6336G touch controller. Is the ft6x06 driver still the newest driver for this controller or is there an alternative (if I create a new TouchGFX project with TouchGFX Designer this driver is also loaded).
Are there any solutions for this behaviour? Thanks.
Julian