Access modelListener and model in a singletone class
I have created a singletone class CommonUtils.cpp because I needed various functions to be used in various part of the code.
It is a very simple class like:
.cpp
#include <gui/common/CommonUtils.hpp>
CommonUtils& CommonUtils::getInstance()
{
static CommonUtils instance;
return instance;
}.hpp
#ifndef COMMONUTILS_HPP
#define COMMONUTILS_HPP
#include <touchgfx/hal/Types.hpp>
#include <touchgfx/Unicode.hpp>
#include <gui/model/ModelListener.hpp>
class CommonUtils : public ModelListener
{
public:
// Get singleton instance
static CommonUtils& getInstance();
// Delete copy constructor and assignment operator
CommonUtils(const CommonUtils&) = delete;
CommonUtils& operator=(const CommonUtils&) = delete;
private:
// Private constructor
CommonUtils() = default;
~CommonUtils() = default;
protected:
Model* model = nullptr;
};The class has various public function that can be call in various part of the code with
CommonUtils::getInstance().myFunction();As you may have seen from the code, I have correctly linked the model to my singleton class adding the bind function and in the FrontedApplication.cpp
#include <gui/common/FrontendApplication.hpp>
#include <gui/common/CommonUtils.hpp>
FrontendApplication::FrontendApplication(Model& m, FrontendHeap& heap)
: FrontendApplicationBase(m, heap)
{
CommonUtils::getInstance().bindModel(&m);
}In this why I can access the model->functionInModel
Now, I would like to be able to access the modelListener as well on my singletone class.
Is there a way to do that?