Skip to main content
GMeta.1
Associate III
August 22, 2024
Solved

Add name of container for items in screen

  • August 22, 2024
  • 1 reply
  • 745 views

It would be useful if an item (widget) added to a screen which is a container, showed the name of the container in the properties window. I have a lot of different containers and if I need to make changes to the container, sometimes I have to go through almost the whole list of containers to find the one I need. If the properties window in the top right of the designer window showed the name of the container, then this would be easier

Maybe also a quicker way to jump to the container either from the screens tab (context menu for example) or via the widget properties window. It is useful btw having an appropriate icon for each widget in the screens tree because you can at least tell if it is a button, line, container etc

Best answer by LouisB

Hello @GMeta.1,

I'm not sure to understand it fully, there's already the name of the custom container in the properties :

LouisB_0-1724757958403.png

 

Best Regards,

1 reply

LouisBBest answer
ST Employee
August 27, 2024

Hello @GMeta.1,

I'm not sure to understand it fully, there's already the name of the custom container in the properties :

LouisB_0-1724757958403.png

 

Best Regards,

GMeta.1
GMeta.1Author
Associate III
August 30, 2024

Hi

OK maybe that was added recently. I am using version 4.19.1 and it doesn't have that:

touchgfx1.png