Adding a new board into TouchGFX Desginer
Hi
I am developing a product based STM32 Microcontrollers. To start with the I am using a Development Board
Nucleo H7A3AI Board.
What I plan to do is, attach a LCD TFT Display to this and develop the prototype. I plan to use TouchGFX designer to develop a UI and develop the firmware
One Problem I face to start with TouchGFX Designer is the development board Nucleo H7A3AI is NOT listed in the supported boards. (I am using TouchGFX Designer 4.25.1 )
The boards which are listed in TouchGFX Designer all have an attached display. In my case we are developing product based on Nucleo H7A3AI Board (This board does not come with a LCD Display).
In such case how can I add my board (Nucleo H7A3AI Board) into TouchGFX Designer ?
The display I am planning to use is From RockTech Model number (RK043HN10E-T)The pin connections
between the display and Nucleo H7A3AI Board is shown below.
| Si.No | Connector Pin No | DISPLAY PIN | STM32H7A3ZI-Q(LCD) |
| 1 | 5 | R0 | PE0 |
| 2 | 6 | R1 | PA2 |
| 3 | 7 | R2 | PC10 |
| 4 | 8 | R3 | PB0 |
| 5 | 9 | R4 | PA5 |
| 6 | 10 | R5 | PC0 |
| 7 | 11 | R6 | PA8 |
| 8 | 12 | R7 | PE15 |
| 9 | 13 | G0 | PB1 |
| 10 | 14 | G1 | PE6 |
| 11 | 15 | G2 | PA6 |
| 12 | 16 | G3 | PC9 |
| 13 | 17 | G4 | PB10 |
| 14 | 18 | G5 | PB11 |
| 15 | 19 | G6 | PC7 |
| 16 | 20 | G7 | PG8 |
| 17 | 21 | B0 | PE4 |
| 18 | 22 | B1 | PD0 |
| 19 | 23 | B2 | PA3 |
| 20 | 24 | B3 | PD10 |
| 21 | 25 | B4 | PC11 |
| 22 | 26 | B5 | PB5 |
| 23 | 27 | B6 | PA15 |
| 24 | 28 | B7 | PD2 |
| 25 | 30 | CLK | PB14 |
| 26 | 32 | VSYNC | PA4 |
| 27 | 33 | HSYNC | PC6 |
| 28 | 34 | DE | PC5 |
| 29 | 31 | DISP | PF9 |