Skip to main content
Associate
October 31, 2023
Question

Bug with TouchGFX designer and nucleo-G071RB + GFX01M2

  • October 31, 2023
  • 2 replies
  • 1362 views

When I create a gauge with this configuration, it works fine in the simulator, but on the device the needle is not visible.

Arcs work fine, and gauge is correctly displayed. Needle is not.

I have tried with STM32F746G-DISCO: it works fine.

It's only with nucleo-G071RB + GFX01M2.

My environment:

- nucleo-G071RB board

- X-NUCLEO-GFX01M2 espansion board (XNGFX01M2$AZ1)

 

2 replies

ST Employee
November 3, 2023

Hello @nbenm ,

Unfortunately, G071RB is not graphically strong enough to handle Texture Mapper animations. That's why the needle is not shown, it is not a bug.
Good luck, don't hesitate to ask more questions

Associate II
April 9, 2025

There is a video of a ST engineer using the gauge widget for reading voltage and temperature. Is that fake? I bought the same board thinking of something similar to this. STM32 Graphics: Getting Started with the Gauge Widget, Part 1  Here is the video. 

ferro
Lead
April 9, 2025

"Is that fake?"

Probably not as in part 2 video the code runs on the board.

 

STM32 Graphics: Getting Started with the Gauge Widget, Part 2

https://www.youtube.com/watch?v=_Usao5UjUSQ

 

I will buy the board as well - I wonder what can be achieved with such a tiny MCU.

ferro_0-1744188178550.png

 

 

nbenmAuthor
Associate
November 3, 2023

Thanks for your answer.

I have the same issue with a STM32F411RE board.

Is it the same reason?

ST Employee
November 6, 2023

You're very welcome.
Yes, if you want such animations you should consider a board from H7 or F7 family