Building the bootloader program auto generated by the touch gfx
When a new project is being created using Touch GFX, the project folder contains a sub-folder ExtMeM_Boot. This folder contains the source files and includes of the bootloader and its dependencies. A pre-built binary is also included (bootloader.bin) which is called by the linker script. The board that I'm using is a STM32H750 Dev - Kit.
My requirement is I need to perform some modifications to the bootloader program (main.c) and rebuild it to generate binary. Is there a method to build the bootloader program simultaneously with the main application or should I move all the contents and its dependencies to new project or is there any other standard method.
Thankyou.