Changing I/O pin function in Riverdi example causes build error
I am using a Rivierdi display with their board that uses a STM32H757XIH6. I am using touchgfx and starting with their pre-made example in touchGFX. Their board has a 40 pin connector that give access to I/O. I am using their project as a starting point and trying to change I/O functions to simple GPIO from alternate function however when I make this change, the project ceases to build. Here is a specific example:
I changed PD11 to GPIO output from LPTIM2_IN2 using pinout view:

I then generated code in CubeMX and tried to build the new project in CubeIDE. The project built fine before the change but failed after this with the following error:
make: *** No rule to make target 'C:/TouchGFXProjects/Regal_shutoff/CM7/Core/Src/lptim.c', needed by 'Application/User/Core/lptim.o'. Stop.
What do I need to do to clear this?