Skip to main content
Bubbly_Bee
Associate
May 21, 2025
Question

Duplicit include paths are added to Keil project when TouchGFX project is regenerated

  • May 21, 2025
  • 1 reply
  • 272 views

Hi,

I have TouchGFX project for MDK-ARM V5.27 toolchain. I am using TouchGFX Designer 4.25.

In Keil project, I have added some additional Include paths. When I need to do some change in GUI and I re-generate code from TouchGFX Designer, IncludePaths in Keil project (uvprojx) are modified in a way that the same paths are added 3 or 4 times.

For example, before re-generating TouchGFX project there is 10 paths which every path is just once here (as I manually delete duplicities). After code generation from TouchGFX Designer, there is 35 paths and some of them are here 4 times, after another regen it´s 60 paths, some of them 8 times ...

Project is compileable, so it´s not problem in this way, but:

  • it makes includePaths really messy 
  • there is change in commit which is badly readable, and it´s absolutely useless
  • project file size is growing

I have tried to find some pattern in that, but I absolutely have no clue why it happens. Definitely, I have some problem in project. But I would like to ask how is TouchGFX generating this list of include paths, to get some hints what to change to stop that behavior.

1 reply

GaetanGodart
Technical Moderator
June 3, 2025

Hello @Bubbly_Bee ,

 

Can you tell me what hardware you are using?

I was not able to reproduce this issue on STM32H753-dk board.

Also, I don't think I ever seen someone talk about a similar issue.

Can you share with me the steps to reproduce the issue?

 

Regards,