Feature request: Stadium button
1) Using the definition I found here (Wolfram-Stadium).
Would it be possible to add an option in the flex button to change into a flex-Stadium/button?
I ask this because I saw multiple implementation of keyboards and most of them instantiate way to many object around the idea of a button (4 corners png , text, callbacks).
2)(extra) I ask this because because you can't easily "stylise" a keyboard via Designer.
It feels like it is easier to just program them manually at the screen setup (i.e.: Gaetan's T9KeyboardCustomWidget).
1b) The only obvious thing that I see is to set a radius_pixel and that would limit the minimal size to not be smaller than a circle. Not sure if customizing the edge with a custom spline would make sense (easing function from the Academy videos).