Skip to main content
Associate
April 19, 2025
Question

Help with Slide Menu

  • April 19, 2025
  • 1 reply
  • 482 views

Hi there,

I'm new to STM32 and was successful to setup a 800x480 LCD with a STM32H743 and SDRAM as Framebuffer.

Now I'm stuck with desiging the GUI with TouchGFX. I would like to add the Slide Menu Option to my screen, however when I press on the assigned button nothing happens in the simulator. I looked at the Slide Menu example but I can't see a difference to my setup. Could someone also have a look at my configuration?

 

always_energized_0-1745084019995.png

 

always_energized_1-1745084094640.png

 

 

1 reply

MM..1
Chief III
April 20, 2025

Seems cant work without background image defined...

Associate
April 20, 2025

Thanks for the Input, now the defined background slides in, however the buttons don't appear. It seems they are covered by the background?

My configuration now looks like this:

always_energized_0-1745150110997.png

 

 

always_energized_2-1745150217878.png

I marked the slide Menu with my cursor.

Any help would be appreciated.

GaetanGodart
Technical Moderator
April 23, 2025

Hello @always_energized ,

 

Can you please share your full project as a 7z file (zipped file)?

 

Regards,