I CANNOT WRITE DATA TO EXTERNAL FLASH WHILE STM32H750 TOUCHGFX IS RUNNING
STM32H750 EXTERNAL FLASH WRITE DATA PROBLEM
Hello everyone,
I am working on a TouchGFX project using STM32H750. In order for the program to be executed, I started the program on the external flash at address 0x90000000 using the bootloader. My project works perfectly for now and I can do everything I want via TouchGFX. I use a 10.1 inch screen. I use MT25QL512ABB8ESF as an external flash and IS42S32400F-6TL as an external RAM. My real problem starts from here. In the later stages of the project, I want to write different data to the external flash whenever I want. And I also want to update the application via WiFi or USB. In order to do these, I need to be able to write data to the external flash while TouchGFX is running. I haven't figured out how to do this yet. Can you help me with this?