Is it possible to capture the screen image with the STM32F4 MCUs?
Hello,
I'm starting a project with an STM32F429IIT6 MCU, but I have a doubt. The project will have a display (I haven't decided yet if it will be 4.3" or 7"), and I'll be controlling the display with the MCU's internal TFT controller using TouchGFX. So far, so good. The issue is that the device needs to be able to capture a screenshot of the screen and save it to an internal microSD. Is this possible, or should I use an external driver to achieve this?
Best Regards, Walter Paz.