Skip to main content
a_niedworok2
Associate II
June 30, 2025
Solved

Is X-NUCLEO-GFX01M2 compatible with NUCLEO-H533RE ?

  • June 30, 2025
  • 1 reply
  • 518 views

Hello!

I wanted to ask if theX-NUCLEO-GFX01M2 module is compatible with STM32 NUCLEO-H533RE? The official documentation does not say anything about this NUCLEO board.

Kind regards 

Andrew 

Best answer by Osman SOYKURT

Hello @a_niedworok2 ,

Yes this X-NUCLEO-GFX01M2 shield is compatible with STM32 NUCLEO-H533RE.

1 reply

Osman SOYKURT
Osman SOYKURTBest answer
Technical Moderator
July 3, 2025

Hello @a_niedworok2 ,

Yes this X-NUCLEO-GFX01M2 shield is compatible with STM32 NUCLEO-H533RE.

Osman SOYKURTST Software Developer | TouchGFX
a_niedworok2
Associate II
July 5, 2025

Thank you for the information.

Is there a driver available for this LCD for the H533?

Andrew

Osman SOYKURT
Technical Moderator
July 9, 2025

The display driver is the same as the other small NUCLEO TBSs (like the NUCLEO-G071RB TBS for instance).
However, if you intend to use the external flash (the one in the display shield), then you would need to create an external loader and use it when flashing your board.

Osman SOYKURTST Software Developer | TouchGFX